DOCA0146EN-07

Firmware Version 003.000.016

New Features

The following features are added:

  • Access through Modbus registers to the trip cause data for MasterPacT MTZ circuit breakers.

  • Aligned display of weekday with MasterPacT MTZ circuit breakers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?