DOCA0146EN-07

Firmware Version 003.001.006

New Features

The following features are added:

  • Access to the legacy dataset for MasterPacT MTZ circuit breakers with the Legacy Dataset Digital Module installed on the MicroLogic X control unit.

  • New signature revocation mechanism to enhance cybersecurity.

Bugs Fixed

Modbus communication parameters of the IFM interface were reset to factory settings after an interruption of the IFM power supply.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?