DOCA0146EN-07

Firmware Version 003.001.010

New Feature

@Updated D1
Access has been added through Modbus registers to the following data for MasterPacT MTZ circuit breakers:

  • Average peak current demand

  • Minimum and maximum values of real-time measurements

  • Energy per phase values

  • Main settings of the active setting group of current protection functions

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?