DOCA0146EN-07

Firmware Version 003.001.012

New Features

The following features are added:

  • New user profiles are added.

  • Reliability improvement of firmware update when IFM interface is stacked with IFE server.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?