DOCA0146EN-07

Firmware Version 003.002.009

New Features

The following features are added:

  • New events to monitor the internal Current Power Supply (CPS) sensors for MasterPacT MTZ circuit breaker.

  • Retry mechanism for optimizing data continuity (automatic bus resynchronization).

Bugs Fixed

The following bugs are fixed:

  • The values in the MasterPacT MTZ circuit breaker dataset were not changed to NA, when MicroLogic was disconnected or IO module source address conflicted.

  • Modbus communication failure with IFM interface was observed when there was unstable power supply.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?