DOCA0146EN-07

Firmware Version 003.002.010

Bug Fixed

The time synchronization of IFM interface with IFE server did not happen when the IFE server was in Daylight Saving mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?