DOCA0146EN-07

Firmware Version 003.002.011

New Features

@updated D1
The new range of ComPacT NSX and PowerPacT H-, J,-, and L- frame circuit breakers are introduced with the evolution of existing Compact NSX and PowerPact H-, J-, and L-frame range of circuit breakers.

Bugs Fixed

The following bugs are fixed:

  • The manufacturing date and time register (11914–11917) showed incorrect seconds information.

  • In IO1 module and M2C status register (32003), bits 9 and 10 showed incorrect M2C status.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?