DOCA0146EN-07

Firmware Version 003.003.000

@New D1 Added the topic for new firmware.

New Features

@Updated D1
The following ground fault protection events are added to IFM interface for MasterPacT MTZ circuit breakers:

  • IDMT ground fault start

  • IDMT ground fault operate

  • IDMT ground fault trip

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?