IFM Interface
Each circuit breaker has its own IFM interface and a corresponding Modbus address.
The IFM interface with part number LV434000 is compatible with the following ranges of circuit breaker:
-
MasterPacT MTZ circuit breakers
-
MasterPacT NT/NW circuit breakers
-
ComPacT NS circuit breakers
-
PowerPacT P- and R-frame circuit breakers
-
ComPacT NSX circuit breakers
-
PowerPacT H-, J-, and L-Frame circuit breakers
-
The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this document applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-Frame circuit breakers in this document applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.
-
These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.