VIGED310023EN-06

Example application: IM15H / IM20-H, HRP, and supervisor

An example of IM15H / IM20-H and HRP installed in the medical premises along with supervisor connected via Modbus communication.

In addition to the features of IM10–H, the IM15H / IM20-H is used to transfer the transformer faults to the HRP. By using Modbus communication (IM20-H ), the operating room staff or maintenance staff is provided with:

  • Insulation value

  • Load level of the transformer

  • Insulation and transformer alarms

  • Timestamped events

The HRP, operation theater cabinet, and supervisor connection is illustrated in the following figure:

The HRP connection principle is illustrated in the following figure:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?