VIGED310023EN-06

Device features

The features supported depend on the device model.
Function IM10-H IM20-H IM15H
Measurement and display of ungrounded system insulation resistance
Threshold-based triggering of alarm
Transformer overload alarm
Transformer high temperature alarm
Time-tagged log (insulation faults, overloads, and transformer overheating events)
Communication via Modbus RS-485
Remote compatibility in operating room (Vigilohm HRP)
Remote compatibility in operating room (Vigilohm Local Remote Display)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?