VIGED310023EN-06

ON light indicator

If the ON light indicator is red, there is an error in the power system or your device.

The error is one of the following cases:

  • Interruption of the injection circuit

  • Auto test not OK

  • Product error

  • System error

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?