VIGED310023EN-06

Operating and alarm LED information

The two bi-color indicator lights on the front panel indicate the device's current status.
ON LED Alarm LED Description
Device powered off
flashes slowly Device powered on, no insulation fault detected
flashes slowly Device powered on, insulation fault detected
Device powered on but malfunctioning
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?