VIGED310023EN-06

Hardware overview

IM10-H ,IM20-H, and IM15H feature 3, 6, and 5 terminal blocks respectively (identifiers A to F).

A Injection connection terminal block
B Auxiliary power supply connection terminal block
C Insulation alarm relay terminal block (IM10-H) / Insulation alarm relay and insulation transformer terminal block (IM15H / IM20-H)
D Terminal block of the 1 A or 5 A input of the CT for measuring the secondary current of the insulation transformer (IM15H / IM20-H)
E Modbus communication terminal block (IM20-H)
F Terminal block for the bimetal input for monitoring the temperature of the insulation transformer (IM15H / IM20-H)
G Contextual menu buttons
H Operating LED
I Insulation alarm LED
J Menu button to go to the main menu
K Esc button to return to the previous menu or cancel a parameter entry
L Display
M Serial number
N Product catalog number (IMD-IM10-H , IMDIM15H, or IMD-IM20-H)

Device commercial reference

Modeld Commercial reference
IM10-H IMD-IM10-H
IM20-H IMD-IM20-H
IM15H IMDIM15H
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?