7EN02-0423-03

Dismounting

  1. Disconnect the terminal blocks from the device.
  2. Insert the blade of a screwdriver between the spring clip and the device and use the screwdriver as a lever to release the spring clip. Release the spring clips at the top and bottom of the device.
  3. Release the 2 spring clips at the side of the device.
  4. Remove the device from the mounting plate.
  5. Reinsert the terminal blocks and make sure that the correct positions on the device are observed (See Hardware overview).
QR code for this page

Was this helpful?