7EN02-0423-03

Injection

Applicable for IM400THRN.

You can set the level of measurement voltage and measurement current that are injected between the monitored power system and ground.

Four setting are available for this parameter:

Value Measurement current value
20V (Default) < 0.469 mA DC
40V < 0.94 mA DC
60V < 1.56 mA DC
80V < 2.48 mA DC

QR code for this page

Was this helpful?