7EN02-0423-03

Primary DC Resistance (Pri. DC Resis)

This parameter is applicable for IM400THRN and when V.Adapt parameter value is set to P1N.

This is the value of resistance of the compatible Schneider Electric voltage transformer primary winding.

You can select any value from 0 to 50 kΩ.

If you have connected more than one transformer, select the value of resistance of single transformer. The device automatically calculates the total resistance depending on the value of the number of transformer parameter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?