7EN02-0423-03

Trend screen

You can view the trends by navigating to Menu > Trend.

An example of Last Day trend page is as follows:

1 Up and down arrows: To view the pages of trend. The pages are Last hour, Last day, Last week, Last month, and Last year
2 Measured value of the insulation resistance
3 Existing value of the insulation alarm threshold
4 Vertical dotted line: indicates a power interruption (duration undefined)
5 Squared area: indicates that the injection has been inhibited

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?