7EN22-0123-04

DLMS/COSEM and ION technologyTechnical Note

This protocol document provides setup instructions for using DLMS/COSEM with PowerLogic™ ION9000 (firmware v2.1.0 and later), ION8650 (firmware v406 and later), ION7400 (firmware v2.1.0 and later) and ION8800 (firmware v350 and later) meters. This document assumes that you are familiar with DLMS/COSEM, your meter and the system in which it is installed.

07/2019

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.