Configuring option module analog inputs using ION Setup
Analog inputs are available on the optional I/O modules.
Calculate your zero scale and full scale values based on the analog source and the input range of your meter.
Make sure that the analog input port that you want to use is properly configured and connected to a valid external analog signal source.
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Navigate to and select the module tab that corresponds to the option module with the analog input you want to configure.
- Select the analog input channel and click Edit. Enter the meter password if prompted. The setup screen for that analog input is displayed.
- Configure the analog input by selecting the parameter and
clicking Edit.
Parameter Value/Range Description Zero scale 0 to ±109 The minimum source value that matches the minimum analog input signal. Full scale 0 to ±109 The maximum source value that matches the maximum analog input signal. Port - The physical analog input port connection. Mode Voltage, current Determines whether the analog input is monitoring voltage or current. Update Rate One Second/High Speed Defines how frequently the input is updated.