Configuring incremental energy using ION Setup
- Start ION Setup.
- Open the Setup Assistant for your meter.
- Navigate to .
- Select Status and click Edit. The Incremental Energy Setup screen is displayed.
- Select Enable to display parameters for configuration.
- Select the parameter to configure.NOTE: Configuring any parameter resets the incremental energy values recorded by your meter.
Parameter Range Description Start time 12:00 am to 11:59 pm The incremental energy first interval’s start time. The start time must be prior to the end time for energy accumulation. End time 12:01 am to 12:00 am The end time for incremental energy.
The end time must be after the start time and be less than or equal to 12AM (midnight).
Interval duration Configurable The increment period for the incremental energy duration. - Click OK to save your changes.