Option 2: Upgrade firmware using individual upgrade files
Meter firmware upgrade to version 2.1.0
The meter firmware upgrade sequence must be strictly followed, as listed:
-
V001.088.000.upg
(PM8000 or ION7400) orV002.000.100.upg
(ION9000 series meters) -
V002.001.000.upx
-
UpgradeAgent_V002.001.000.upx
To retain your meter settings and readings, select a meter template file (DCF) to paste into the meter when performing the first two firmware upgrades.
NOTICE |
---|
lost settings
Always select a template file when upgrading the meter
firmware.
Failure to follow these instructions can result in loss
of meter settings.
|
Use the Template Paste Options box to specify what you want to retain after the upgrade.