SNMP Options Module
Module icon
Overview
SNMP is enabled/disabled based
on the Enable SNMP register in the Communications
module. The SNMP Options module is used with the Alarm Options module
for SNMP trapping. It is a core module that cannot be deleted, copied
or linked. It is configured by altering the contents of its setup
registers.
Inputs
The SNMP Options module has no programmable inputs.
Setup registers
This register enables or disables SNMP trapping on your meter. SNMP must also be enabled in order for SNMP trapping to be enabled. Refer to the Communications module for SNMP enabling.
Trap Rcvr1 Addr...Trap Rcvr4 Addr
These registers specify the IP address and optional port number for the SNMP trap receivers. This value may either be:
-
an IPv4 address in the format of
###.###.###.###:<port>
-
an IPv6 address in the format of
[nnnn.nnnn.nnnn.nnnn.nnnn.nnnn.nnnn.nnnn]:<port>
-
a fully qualified domain name (for example,
snmp.yourcompnay.com:<port>
)
This register specifies the community string used for SNMP get (read-only) requests.
This register specifies the community string used for SNMP set (read/write) requests.
This register specifies the name of the administrative contact.
This register specifies the name of the device.
This register specifies where the device is located.
Output registers
All events are recorded in the Event register. Possible events and their associated priority numbers are:
Event priority group | Priority | Description |
---|---|---|
Setup Change | 10 | Input links, setup registers or labels have changed. |
The Event output register stores the following information for each ION event: time stamp, priority, cause, effect, and any values or conditions associated with the cause and effect.
Responses to special conditions
The following table summarizes how the module behaves under different conditions.
Condition | Response of output registers |
---|---|
When the meter is started or powered-up (either the first time, or after a shutdown). | All output registers retain the values they held when the meter was shutdown. |