SNMP trapping implementation
-
Coldstart: the meter (SNMP agent) is starting.
-
Linkup: the SNMP agent is enabled.
-
AuthenticationFailure: the meter (SNMP agent) has received an incorrect community value.
Enterprise-specific SNMP traps supported by your meter are:
-
Low: trap of events with a low event priority.
-
Medium: trap of events with a medium event priority.
-
High: trap of events with a high event priority.
Trap | Event priority range |
---|---|
Low | 64–127 |
Medium | 128–191 |
High | 192–255 |
See the ION Reference, available from www.se.com, for detailed information on the SNMP Mapping, SNMP Options and Alarm Options modules.