Read Device Registers
Description
This page allows the Link150 gateway to read Modbus registers from the selected device.
Read Procedure
Step |
Action |
Result |
---|---|---|
1 |
On the menu bar, click . |
Opens the menu. |
2 |
From the menu, in the submenu, click . |
Opens the page. |
3 |
Select the device from the list. |
Selects the device from the list. |
4 |
Enter (or choose from the defined device list), , and then . |
Enters the registers to read from the specified device. NOTE: The
parameter is disabled in slave
mode.
|
5 |
Select the . |
Selects the appropriate data type. |
6 |
To change how Modbus data is displayed in the column, select , , , or . |
Selects how the data values are displayed. |
7 |
Click . |
Reads the device register according to the selected configuration. |
Link150 Read Device Register Parameters
Parameter |
Description |
Settings |
---|---|---|
|
Selects a device to read from the list of previously added devices. NOTE: When the device
is in slave mode, the
button is available even if a name is not selected
from the list.
|
- |
|
The address (Local ID) of the device that is to be read. NOTE: The
parameter is disabled in slave
mode.
|
1 (Factory setting) |
|
Register number in decimal. |
|
|
The number of registers to read. |
|
|
Lists the register numbers in decimal. |
- |
|
Lists the data stored for a register. Values retrieved depend on the device connected to the Link150 gateway. Refer to the documentation for the connected device for more information about stored register values. |
- |
|
Lists the data types available for the device. |
|
options |
Selects an option to specify how the column data is displayed. |
Decimal (Factory setting) |