Whole House SPDs

Surgebreaker Plus Whole House Surge Protective Device

SDSB80111

The Surgebreaker Plus Whole House device is designed to deliver surge suppression that addresses the entire home. AC modules are connected to the circuit breaker load center and provide suppression for all equipment connected to the power system. This Whole House system incorporates AC modules as well as modules for other metallic lines coming into the home including telephone/DSL and coaxial video/data.

US and Canadian UL® Listed as Type 2 SPD to the UL 1449 standard. Complies with requirements of NEC® Article 285, CSA 233.1-87, and CSA C22.2 No. 8-M1986 as appropriate. Telephone and coaxial video modules US and Canadian UL® Recognized to UL 497A 4th Edition and UL 497B 4th Edition.


  • 120/240 Vac, 80 kA/phase AC surge suppression

  • LED status indicators for AC surge suppression

  • Telephone surge suppression module supports one RJ45 cable up to four lines.

  • Coaxial surge suppression module supports one line of video/data

  • Network suppression module supports one RJ45 modem/fax/DSL


Whole House Surge Protective Devices

Description

Included Modules

Cat. No.

Whole House NEMA 1

AC, Telephone, Coax, Network

SDSB80111

SDSB80111 Replacement Modules

Description

Cat. No.

Telephone Suppression Module

PTEL2R

Video Suppression Module

PVR

Network Suppression Module

PNETR6

Home Electronics Protective Device

HEPD80

Was this helpful?