MotorSeT™

Class 8198

MotorSeT™ Medium Voltage Motor Controllers (UL Listed)

Coming soon!

MotorSeT™ – The next generation of our Medium Voltage Motor Control Centers.

The offer will be released in several phases. The first waves will be across-the-line (full voltage non-reversing and reversing) starters and reduced voltage soft starters, including 1-high and 2-high designs as well as a compact 20-inch footprint version.

Future waves will include higher voltage versions (> 4, 160 V and up to 7,200 V) rated ATLs and RVSS, and arc-resistant enclosures. Look for updates on MotorSeT on www.se.com/us for additional information and updates on releases.

Was this helpful?