Type SK Corrosion Resistant Multifunction Operators

Class 9001 / Refer to Catalog 9001CT1103

Type SK Corrosion Resistant Multifunction Operators

Multifunction Operators—UL Types 4, 4X, 13/NEMA 4, 4X, 13 [1][2]

Interlocked Assembly

 

Description

Color

Contacts [3]

Without Contacts [3]

9001SKR11U

Interlocked Assembly

Both Buttons Maintained

Universal [4]

SKR11UH1

SKR11U

Other [5]

SKR11▼H1

SKR11▼

Interlocked Assembly

One Button Momentary

Universal [4]

SKR12UH1H1

SKR12U

Interlocked Assembly

One Button Maintained

Other [5]

SKR12▼H1H1

SKR12▼

Footnotes

  1. For use in hazardous locations—See Square D Offering According to Class, Division, and Group.
  2. Legend plate and contact block not included unless otherwise noted.
  3. When ordering, add prefix 9001 to the catalog number.
  4. Universal for SKR11,12 includes 2 each of black, red, green, yellow, orange, blue, white.
  5. ▼ Choose one color for each button. R = red, G = green, B = Black.Example: 9001SKR11 with top button gray and bottom button orange = 9001SKR11ES. See Color Codes

Was this helpful?