XCMD Modular

Refer to Telemecanique Sensors

Overview — Metal

1. Pre-cabled connection components: replace the bullet (●) in the catalog number with the required cable length in meters, either 1, 2, 3, 5, 7 or 10.

Example: ZCMC21L• becomes ZCMC21L7 for a 7 m (23.0 ft) cable.

Note: only cable lengths of 1, 2 and 5 m (3.3, 6.6, and 16.4 ft) are available for pre-cabled connection components ZCMC37L● and ZCMC39L●.

Was this helpful?