XCKJ Industrial Format EN 50041, Fixed or Plug-in Body

Refer to Telemecanique Sensors

Overview — Standard Industrial, Metal

(1) Cannot be used with bodies ZCKJ4H7 and ZCKJ41H7.

(2) For further information, see page 21-27.

(3) For a cable entry tapped ISO M20 x 1.5, change H7 to H29. Example: ZCKJ1H7 becomes ZCKJ1H29.

For a cable entry tapped Pg 13.5, delete H7 from the catalog number. Example: JCKJ1H7 becomes ZCKJ1.

Head assuring positive opening operation when used with a conforming lever.

(4) Adjustable throughout 360° in 5° steps, or in 90° steps by reversing the notched washer.

(5) Adjustable throughout 360° in 5° steps, or in 45° steps by reversing the lever mounting.

(6) Suitable for bodies with contacts ZCKJ1 / J2 / J31 / J39H7.

Was this helpful?