9007C Factory Modifications (Forms)

Refer to Telemecanique Sensors

Factory Modifications

Special Features (do not apply to Type CR unless noted)—Not Field Installable, Except Where Noted

Special Features

Form

Hub

Optional Shaft Equipped With 9007T / 9007FT Hub: Any lever arm Type C, CF, or CR switch can be furnished with an optional shaft and hub combination which will accept the lever arms normally used with Type T and FT limit (position) switches. To order, add S9 as suffix to the device type number. For example, to order a 9007C54B2 with this modification, order as 9007C54B2S9. For details about the switches and lever arms that can be furnished with this modification, see catalog 9007CT1007.

Add S9 as a suffix to the catalog number

Hub Only: Can be field installed on any Type C lever type switch.

Cat. No.

9007S9

LED Pilot Light, 24–120 Vac or Vdc on Plug-In Type Switch (Type C52, C54, C62, C64, C66, or C68):

Addition of LED pilot light in parallel with N.O. contact (light normally on)

P5

Addition of LED pilot light in parallel with N.C. contact (light normally off)

P6

Addition of one isolated LED pilot light (light on when load is energized) (Type C54 only. Not available with Y1901.)

P10

Pre-Wired Receptacle

Single Pole

Plug-in limit (position) switch with pre-wired mini 5 pin male receptacle. For use with Brad Harrison female portable plug No. 41306, 41307, or 41308 (or equal). (Not available with P10 or for hazardous locations.)

Y1901

Same as Y1901 but with different wire color coding

Y1905

Other versions with different wiring diagrams per automotive requirements are available. Contact your local Schneider Electric field office.

Mating plug and cables available.

 

Potted Limit (Position) Switch or Plug-In Receptacle Only:

With Individual Wires

 
  • Single pole plug-in limit (position) switch or receptacle pre-wired with five #16 wires 5 ft long and wire entry completely sealed with epoxy resin

Y1841

With STOWA Cord

 
  • Single pole plug-in limit (position) switch or receptacle pre-wired with five conductor #16 STOWA cord 8 ft long and wire entry completely sealed with epoxy resin

  • Double pole plug-in limit (position) switch or receptacle pre-wired with nine conductor #16 STOWA cord 8 ft long and wire entry completely sealed with epoxy resin

Y1851

Y1852

Other versions with different wiring diagrams for automotive requirements are available.

     

Low Temperature—Lever Types Only: Limit (Position) switch will operate in an ambient temperature range of -40 to +185 °F (standard limit switch ambient temperature
range is -20 to +185 °F). Minimum temperature is based on the absence of freezing moisture or water.

Y128  

Fluorocarbon Rubber (FKM) Gaskets And Seals

Substitute fluorocarbon rubber gaskets and seals on:

  • Lever arm type, standard box (shaft seals on lever arm types are fluorocarbon rubber as standard)

  • Lever arm type, compact box (shaft seals on lever arm types are fluorocarbon rubber as standard)

  • Plunger type, standard box 

  • Plunger type, compact box 

NOTE: Fluorocarbon rubber has been shown to resist sunlight aging problems.

Y140 

Direct Acting Contacts [1]

Substitution of direct acting contact unit for snap switch of single-pole switch:
One pole, normally closed, slow-make slow-break, direct acting contact mechanism substituted for standard snap switch on Types C52, C54, CF53, and CR53 devices.
This mechanism was designed for use in emergency overtravel applications. The movable contact of this basic switch unit is acted upon directly by the actuating mechanism of the limit switch—it does not depend on the force exerted by a snap-switch blade or a spring to open the circuit. Because these contacts are slow-make slow-break, they are best suited for applications where they are not actuated during normal operation, but only if abnormal overtravel is encountered.

Direct Acting Contact Mechanism (shown without cover)

Y1561

Footnotes

  1. The direct acting contacts described above come standard on the 9007CLS1 hoist overtravel switch.

Was this helpful?