Class 9012G Dimensions

Class 9998 / Refer to Catalog 9012CT9701

Dimensions

9012G Dimensions, in. (mm)

9012GNO1, GRO1

9012GNG1, GRG1

   

9012GNO, GRO

9012GNG, GRG

Type

Dimension A, in. (mm)

GNO, GRO 3, 4, 5, 6

1.41 (35.8)

GPO, GSO 1, 2, 3

1.31 (33.3)

GQO, GTO 1, 2, 3, 4

2.24 (56.9)

Type

Dimension A, in. (mm)

GNG, GRG 3, 4, 5, 6

1.41 (35.8)

GPG, GSG 1, 2, 3

1.31 (33.3)

GQG, GTG 1, 2, 3, 4

2.24 (56.9)

Was this helpful?