PacDrive 3 Automation Solution

PacDrive 3

PacDrive Family

PacDrive 3 is based upon proven logic motion technology, which unifies PLC, motion, and robotics control functionality on a single hardware platform. With its centralized system architecture, PacDrive 3 is the ideal solution for controlling a broad range of servo-driven production and packaging machines, as well as material handling equipment and robotics, using fully integrated, IEC 61131-3-compliant program structures. More than 80.000 machines worldwide are controlled by PacDrive to this day.

PacDrive 3 Robotics

Lexium T and Lexium P Delta Robots

Lexium STS SCARA Robots


Links to Websites and Downloads:

PacDrive 3

Motion Sizer (Free) Software

EcoStruxure™ Machine Expert Programming Software

Was this helpful?