Shielding and Grounding

The automation network shield should be grounded in one place only, typically at the RS232/485 converter as shown in Alternate RS485 Wiring.

The controller circuitry and associated Class 2 wiring is electrically isolated from all system voltages and earth ground. Maintaining the integrity of this isolation is important for proper operation and performance.

The controller’s input terminals and auxiliary power source are part of the Class 2 circuitry. External devices connected to the controller must meet the isolation requirements and other Class 2 wiring standards. Do not connect the controller to external voltage sources or earth ground.

The RS485 network communications circuit is also part of the Class 2 circuitry. In most applications, the shield of each communications cable will be interconnected at the center terminal of the communications connector. This connection ensures networked controllers are tied together to a common reference potential. The shield must be grounded at only one point in the system. Grounding the shield at multiple points will create a “ground loop” that may disrupt communications or cause damage to the controller circuitry.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?