BQT2027101-01

Controller Set Up

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
Never reduce the steps connection time under 50 s.
Failure to follow these instructions will result in death or serious injury.
NOTICE
DEGRADATION OF EQUIPMENT PERFORMANCE
The controller is configured in the factory for normal or optimal operation. The user is liable for any modification of these parameters.
Make sure that the MCCB (Molded Case Circuit Breaker) and thermostat settings are not altered without proper authorization or expertise.
Failure to follow these instructions will lead to the total or partial loss of the equipment and unavailability of the installation.

External View of Powerlogic PFC Controller VPL6/VPL12

Display

Navigation Keys

 
  1. Display

  2. Navigation keys

  3. Digital display for measurement

  4. Displacement Power Factor (DPF)

  5. Inductive or capacitive DPF (lagging or leading)

  6. Units of measurement

  7. Step information

  8. Indicates automatic mode

  9. Indicates manual operation of steps mode

  10. Indicates set up menu mode

  11. Flashing indicates alarm is activated

  12. Step number illuminated when activated

  13. Displayed measurement

  14. Indicates exporting power to grid

  15. Indicates secondary DPF target is activated

  16. Increase Values/Select Menu Items

  17. Open Menu/Move Cursor Right/Settings

  18. Decrease Values/Select Menu Items

  19. Exit Menu/Move Cursor Left

The regulator installed in your Powerlogic PFC Capacitor Bank pre-configured with your equipment, following settings have to be defined:

  • Target cos φ setting

  • Current transformer ratio value (allows to display the measured value correctly)

NOTE: For more detailed information on the controller, refer to the device manual supplied with the equipment.

Important

  • If supplied by a summing CT (installation with several CTs), the sum of the ratios of the different CTs must be taken into consideration.

  • For an installation equipped with a generator set, the capacitor bank must be taken out of circuit, by breaking the supply to the controller, before switching to the generator set.

NOTE: For controller operation, refer to the instructions supplied with the product.

Simple Commissioning of PowerLogic PFC Controller

Before configuring the controller, make sure that the jumper on KL terminals is removed.

Go to SETUP 100:

  1. Setup CT ratio (Ct), cos φ (CP1).

  2. If the controller display is showing PFC OFF, set the PFC parameter to ON, before launching Ai.

  3. Launch Automatic Initialization (Ai) by pressing Ai from OFF to ON.

The Ai automatically detects the capacitor steps connected and checks if the phase connection (angle between voltage and CT position) is correct. The Ai sequence switches the steps on and off several times. It will take several minutes to complete this process, and later the relay will stabilize.

During this sequence, the controller will display Ai.

Minimum Requirements to Launch an Ai

Following are the minimum requirements to launch an Ai:

  • Voltage must be within tolerance

  • CT must be connected

  • Capacitor protection must be closed

  • Input current not too low

For a Successful Ai Step Detection

  • Current loading shall be significant

  • Load variation shall not be significant

Successful Ai Sequence Information

  • If phase wiring is swapped (incorrectly wired), the controller automatically corrects the phase angle internally and moves to normal mode. Auto is displayed.

  • Final check of step detection:

    • Go to SETUP 100 > OUT > open (right arrow) and check if the status of all steps are correct as per the PFC bank configuration (FIX OFF= Step not detected. AUTO= Step detected).

    • If necessary, change the OUT status to expected value.

Unsuccessful Ai Sequence [“Abrt” (abort) error]

If unsuccessful, run the Ai again. If the Ai aborts again, the phase connection (angle between voltage and CT position) cannot be detected. The control will move to PFC off mode and phase connection must be set manually. See PowerLogic™ VL series PF Correction Controller User Manual.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?