BQT2027101-01

Introduction

Powerlogic PFC (Power Factor Correction) Capacitor Bank is a low voltage energy-efficiency equipment designed to optimize the power factor of electrical systems, provides efficient energy usage and minimizing power wastage. Power factor is a critical factor in electrical systems, representing the ratio of real power (active power) to apparent power (the combination of real and reactive power). A low power factor results in increased current flow, higher energy losses, and reduced electrical efficiency.

The Powerlogic PFC Capacitor Bank is engineered to counteract this issue by providing reactive power, effectively balancing the power factor and improving system efficiency. It achieves this by supplying reactive power in the form of capacitive reactive current. By doing so, it helps to reduce the overall current drawn from the electrical supply and diminishes losses, ultimately enhancing the systems power factor.

The Powerlogic PFC Capacitor Bank typically consists of a series of capacitors that can be switched on or off based on the systems real-time power factor requirements. These capacitors are intelligently controlled by a power factor controller, which monitors the power factor and activates or deactivates the capacitors as needed to maintain an optimal power factor level.

Benefits

Installing a Powerlogic PFC Capacitor Bank in an electrical system offers numerous advantages, including:

  • Improved energy efficiency: By raising the power factor, the system can operate more efficiently, reducing energy consumption and lowering electricity costs.

  • Reduced electricity bills: Power utilities often penalize consumers for low power factors, so maintaining a higher power factor can result in lower utility charges.

  • Increased system capacity: The reduction in reactive power flow allows the electrical system to handle more active power, increasing its overall capacity.

  • Extended equipment lifespan: Lower current levels lead to less stress on electrical components, contributing to increased equipment lifespan and reduced maintenance costs.

  • Environmental benefits: An improved power factor results in lower overall power consumption, which can help reduce greenhouse gas emissions and environmental impact.

Overall, the Powerlogic PFC Capacitor Bank is an essential equipment for industries, commercial facilities, and large-scale consumers of electricity seeking to optimize their power factor and enhance their energy efficiency. By mitigating power losses and optimizing electrical systems, this technology plays a crucial role in creating a more sustainable and cost-effective electrical infrastructure.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?