BQT2027101-01

Technical Characteristics

General Characteristics

The following are the general characteristics of the Powerlogic PFC Capacitor Bank:

  • Voltage, frequency, and power as per rating plate

  • Insulation voltage: 690 V

  • Conditional short circuit current: 50 kA

  • IP protection rating: VLF1P (IP41), VLF2P (IP42), and VLF3P (IP42)

  • Colour (cubicle): RAL 7035

  • Compliant with IEC 61439-1/2 and IEC 61921

  • Impact protection: IK10

Characteristics of the Capacitors

The following are the characteristics of the Capacitors used in Powerlogic PFC Capacitor Bank:

  • Rating tolerance: -5...+10%

  • Permissible voltage overload (8 hours out of 24 hours as defined in IEC 60831-1/2): 10%

Operational Limits

The following are the operational limits of the Powerlogic PFC Capacitor Bank:

  • Indoor use only

  • Power supply: 400 V/50 Hz and 415 V/50 Hz

Rating Plate

PowerLogic PFC Capacitor Bank Wiring Diagram

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?