Cost management

Your device can be used in various cost management applications.

Some of the applications are as mentioned below:

  • Measurement of basic electrical parameters in control panels, power distribution boards, OEM’s, Building management systems, and panel instrumentation

  • Aggregate energy consumption and cost allocation based on consumption from Utility vs Genset, or between any two power sources, per area, per shift, and per time within the same facility

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?