Demand setup

Demand is a measure of average consumption (power) over a fixed programmed time interval.

You can view the demand values provided in Demand page by navigating through display parameters. The meter supports editing power demand through Setup mode.

To view demand setup values, follow these steps:

  1. From the Home page, use Up or Down button to navigate to Maintain.
  2. Press OK.
  3. Use Up or Down button to navigate to Set.
  4. Press OK.
  5. Enter password. Default password is 0000.
  6. Press OK.
  7. Select the parameter from the list. Press the Down button to select Pd (power demand method), Pd.Cy (demand period), Pd.ut (demand update time), or Pd.P (demand parameter).
  8. Press OK.
  9. Press the Down button to select required values from the list.
  10. Press OK.
  11. Press Left button.
  12. Select Yes (Press OK button) to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?