Firmware upgrades

There are a number of reasons why you may want to upgrade your meter’s firmware.

Some of the reasons are mentioned below. It is suggested to keep your meter firmware upgraded for optimum performance.

  • Improve meter performance (e.g., optimize processing speed)

  • Enhance existing meter features and functions

  • Add new functionality to the meter

  • Achieve compliance to new industry standards

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?