Keypad operation PM1130H

Press a key in the direction you want to go. The display shows the next parameter as per navigation. Press OK to enter a parameter setup.

The following steps explain how to navigate from the RMS page to the VLN A F page and back to RMS page.

  1. From the RMS page, press right button. The display shows VLL W PF.

  2. Press down button. The display shows VLN A F.

  3. To return to RMS, press left bottun. The display shows RMS.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?