Meter types
| Commercial reference | Description |
|---|---|
|
METSEPM1130HCL05RS METSEPM1130HCL05RD METSEPM1130HCL05VN |
Class 0.5 panel mount meter with relay, alternate source, RS-485, and integrated display. |
|
METSEEM6438HCL05RS |
Class 0.5 panel mount meter with alternate source, RS-485, and integrated display. |
|
METSEEM6438HCL10RS |
Class 1 panel mount meter with alternate source, RS-485, and integrated display. |
|
METSEPM1130HCL5LVD |
Class 0.5 panel mount meter with low voltage DC, relay and alternate source, RS-485 and integrated display |
|
METSEPM1140HCL5 |
Class 0.5 panel mount meter with relay, digital input, RS-485, and integrated display. |
|
METSEPM1140HCL1 |
Class 1 panel mount meter with relay, digital input, RS-485, and integrated display. |