Common hazard statement elements

-
NOTE
DO NOT MAKE ANY CHANGES TO THIS TOPIC
THE CHANGES TO THIS TOPIC IS MANAGED VIA COMMON CONTENT CHANGE PROCESS. REFER TO https://schneider-electric.app.box.com/folder/49532687642

Use these common hazard messages, statements of hazard and avoidance bullets in your safety messages.

Main safety precautions preamble, hazard, avoidance bullets and post-steps

Installation, wiring, testing and service must be performed in accordance with all local and national electrical codes.

  1. Turn off all power supplying this device and the equipment in which it is installed before working on or in the equipment.

  2. Always use a properly rated voltage sensing device to confirm that all power is off.

Preambles

If you lose your password, you must return the meter for factory reconfiguration, which resets your device to its factory defaults and destroys all logged data.

Hazard statements

HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH

Data Loss

Unintended Operation

Irrecoverable password

Inaccurate data results

Equipment damage

Permanently locked device

Potential compromise of system availability, integrity, and confidentiality

IP ADDRESS CONFLICT

Avoidance statements

Apply appropriate Personal Protective Equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462 or other local standards.

Turn off all power supplying this device and the equipment in which it is installed before working on or in the equipment.

Always use a properly rated voltage sensing device to confirm that all power is off.

Assume communications and I/O wiring are hazardous live until determined otherwise.

Do not exceed the maximum ratings of this device.

Do not short secondary terminals of Voltage Transformer (VT).

Do not open secondary terminals of Current Transformer (CT).

Ground secondary circuit of CTs.

Do not use this device for critical control or protection of persons, animals, property or equipment.

Connect protective ground (earth) before turning on any power supplying this device.

This meter can only be used as a permanently installed device with permanent electrical connections including earth ground.

Replace all devices, doors and covers before turning on power to this equipment.

Do not use this device for critical control or protection of persons, animals, property or equipment.

Verify the device’s power source meets the specifications for your device’s power supply.

Save the contents of the data log before configuring it.

Do not rely solely on data displayed on the display or in software to determine if this device is functioning correctly or complying with all applicable standards.

Do not rely solely on data displayed in the software reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.

Do not use data displayed on the display or in software as a substitute for proper workplace practices or equipment maintenance.

Do not use data displayed in the software as a substitute for proper workplace practices or equipment maintenance.

Verify that associated devices and ION Setup are configured correctly.

Confirm your alarm is properly configured.

Only use CAT5/5e/6/6a cables with unshielded plugs.

Only use unshielded CAT5/5e UTP Ethernet cables.

Save your meter's data before performing a reset.

Record your device's user and password information in a secure location.

Do not exceed the maximum number of option modules.

Ensure you maintain sufficient access to communicate to and configure your device.

Ensure that all important data has been recorded before uploading firmware or a template to your device.

Save the contents of the data log before configuring it.

Change default passwords to help prevent unauthorized access to device settings and information.

Disable unused ports/services and default accounts, where possible, to minimize pathways for malicious attacks.

Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).

Use cybersecurity best practices (for example: least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, interruption of services, or unintended operation.

Do not use the data from the meter to confirm power is off.

Disconnect the injection wire from the device to the monitored system before working on the device or equipment.

Never shunt an external fuse or circuit breaker.

Do not use ION devices or software for critical control or protection applications where human or equipment safety relies on the operation of the control circuit.

Ensure the analog input is configured for the correct voltage or current mode before connecting or activating the analog transducer.

Ensure that your ungrounded system has a compatible insulation monitoring device.

Disconnect all the device’s input and output wires before performing dielectric (hi-pot) or Megger testing.

Disconnect all power and measurement wiring before working on this device.

Do not connect a Com'X Ethernet port to a local area network if it is configured to DHCP server.

Do not open the device case.

Do not attempt to repair any components of the device.

Use only Low Power Current Transformers (LPCTs) that are approved for use with this device.

Do not connect CT secondary signals to meter low voltage LPCT terminals.

Do not install CTs or LPCTs in equipment where they exceed 75% of the wiring space of any cross-sectional area in the equipment.

Do not install CTs or LPCTs in areas where ventilation openings may be blocked or in areas of breaker arc venting.

Do not install CTs or LPCTs using Class 2 wiring methods or connect to Class 2 equipment. See NFPA 70.

Secure CT or LPCT secondary conductors to ensure they do not contact live circuits.

Follow guidelines in the Wiring section of the related Installation Sheet.

Change default passwords/passcodes/PIN codes to help prevent unauthorized access to device settings and information.

Do not use this device if a wrench icon appears on the top corner of the display screen or if the value under Meter Status is not “OK”.

Use copper conductors only.

Notice consequence statements (all other message types have the failure to follow automatically filled in)

Failure to follow these instructions can result in data loss.

Failure to follow these instructions can result in loss of access to the device.

Note used in Safety Precautions

NOTE: See IEC 60950-1 for more information on communications and I/O wiring connected to multiple devices.
NOTE: See IEC 60364-4-41 for more information on protection against electrical shock.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Contenu utile ?