Configuring BACnet/IP settings using the display
- Navigate to .
- Enter the setup password (default is “0”),then press OK.
- Navigate to .
- Move the cursor to point to the parameter you want to modify, then press Edit.
- Modify the parameter as required, then press OK.
- Move the cursor to point to the next parameter you want to modify, press Edit, make your changes, then press OK.
- Press the up arrow to exit.
Basic BACnet/IP settings available using the display
Parameter Values Description BACnet Status
Enabled, Disabled
Enable or disable BACnet/IP communications with the meter
Device ID
0 – 4194302
Enter the ID of the meter on your BACnet network. The ID must be unique on the network.
UDP Port
1024 – 65535
Enter the port the meter uses for BACnet/IP communications. The default is the standard BACnet/IP port (47808).
Foreign device settings available using the display
Parameter Values Description BBMD Status
Enabled, Disabled
Enable or disabled registration of the meter as a foreign device.
BBMD IP
Contact your local network administrator for parameter values.
Enter the IP address of the BACnet/IP Broadcast Management Device (BBMD), if you use a BBMD on your network.
BBMD Port
1024 – 65535
Enter the port number that is used for communications with the BBMD. The default is the standard BACnet/IP port (47808)
BBMD TTL (sec)
0 – 65535
The length of time (in seconds) the BBMD keeps an entry for this device in its foreign device table.