EAV15107-EN09

Configuring the energy scaling using ION Setup

You can use ION Setup to configure the energy scaling. Based on the scaling, the energy overflow happens upon reaching the threshold value.
  1. Start ION Setup.
  2. Connect to your meter.
  3. Open the Energy Scaling screen.
  4. Click Edit to configure the Setup parameters as required.
  5. Use the drop-down list to select the parameter you want to set for your Energy Scaling.
    NOTE: If you set Energy Scaling parameter, for which the threshold value is less than the accumulated energy, the accumulated energy resets to zero.
  6. Click Send to save your changes to the meter.

    Energy Scaling parameters available using the ION Setup

    Parameter

    Values

    Description

    Auto

    (Default)

    0 to 9.2233 E

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega, Mega to Giga, Giga to Tera, Tera to Peta and Peta to Exa.

    When any one of the energy parameter (delivered or received) exceeds 9.2233 E, all the energy parameters reset to 0.

    Kilo (k)

    0 to 999.99 k

    When any one of the energy parameter (delivered or received) exceeds 999.99 k, all the energy parameters reset to 0.

    Mega (M)

    0 to 999.99 M

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega.

    When any one of the energy parameter (delivered or received) exceeds 999.99 M, all the energy parameters reset to 0.

    Giga (G)

    0 to 999.99 G

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega and Mega to Giga.

    When any one of the energy parameter (delivered or received) exceeds 999.99 G, all the energy parameters reset to 0.

    Tera (T)

    0 to 999.99 T

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega, Mega to Giga and Giga to Tera.

    When any one of the energy parameter (delivered or received) exceeds 999.99 T, all the energy parameters reset to 0.

    Peta (P)

    0 to 999.99 P

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega, Mega to Giga, Giga to Tera and Tera to Peta.

    When any one of the energy parameter (delivered or received) exceeds 999.99 P, all the energy parameters reset to 0.

    Exa (E)

    0 to 9.2233 E

    The energy value units automatically change, based on the quantity of energy accumulated, from Kilo to Mega, Mega to Giga, Giga to Tera, Tera to Peta and Peta to Exa.

    When any one of the energy parameter (delivered or received) exceeds 9.2233 E, all the energy parameters reset to 0.

QR code for this page

Was this helpful?