EAV15107-EN10

Cybersecurity overview

This chapter contains up-to-date information about your product’s cybersecurity. Network administrators, system integrators and personnel that commission, maintain or dispose of a device should:

Your device has security capabilities that:

  • Allow it to be part of a NERC CIP compliant facility. Go to the North American Electric Reliability Corporation website for information on NERC Reliability Standards.

  • Align with cybersecurity standards in the IEC 62443 international standard for business IT systems and Industrial Automation and Control Systems (IACS) products. Go to the International Electrotechnical Commission website for information about the IEC62443 international standard.

To communicate a security topic affecting a Schneider Electric product or solution, go to http://www.se.com/en/work/support/cybersecurity/vulnerability-policy.jsp.

WARNING
Potential compromise of system availability, integrity, and confidentiality
  • Change default passwords to help prevent unauthorized access to device settings and information.
  • Disable unused ports/services and default accounts, where possible, to minimize pathways for malicious attacks.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example: least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, interruption of services, or unintended operation.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
QR code for this page

Was this helpful?