EAV15107-EN09

Ethernet communications connections

Use a shielded Ethernet cable to connect the meter’s Ethernet port.

Ground terminal is not available on the meter; shield should be connected to ground at the other end. Your Ethernet connection source should be installed in a location that minimizes the overall Ethernet cable routing length.

QR code for this page

Was this helpful?