EAV15107-EN11

Meter Initialization

Meter Initialization is a special command that clears the meter’s logged data, counters and timers.

It is common practice to initialize the meter after its configuration is completed, before adding it to an energy management system.

After configuring all the meter setup parameters, navigate through the different meter display screens and make sure the displayed data is valid then perform meter initialization.

QR code for this page

Was this helpful?