EAV15107-EN11

Performing global resets using the display

Global resets allow you to clear all data of a particular type, such as all energy values or all minimum/maximum values.
  1. Navigate to Maint > Reset.
  2. Move the cursor to point to Global Reset, then press Select.
  3. Move the cursor to point to the parameter you want to reset, then press Reset.
    Option Description
    Meter Initialization Clears all data listed in this table (energy, demand, min/max values, counters, logs and timers).
    Energies Clears all accumulated energy values (kWh, kVARh, kVAh).
    Demands Clears all the demand registers.
    Min/Max Clears all the minimum and maximum registers.
    Alarm Counts & Logs Clears all the alarm counters and alarm logs.
    I/O Counts & Timers Clears all the I/O counters and resets all the timers.
  4. Enter the reset password (default is “0”), then press OK.
  5. Press Yes to confirm the reset or No to cancel and return to the previous screen.

    To perform resets using ION Setup, see the “PM5300” topic in the ION Setup online help or in the ION Setup device configuration guide, available from www.se.com.

QR code for this page

Was this helpful?