HRB1684301-16

Acknowledging high-priority alarms using the display

You can use the meter display to acknowledge high-priority alarms.
**is this accurate? only high-priority alarms?
  1. Navigate to Alarm > Unack .
  2. Select the alarm you want to acknowledge.
  3. Press Detail.
  4. Press Ack to acknowledge the alarm.
  5. Repeat for other unacknowledged alarms.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?